Menu
Recent Webcast

3kW Fiber Laser Launched by JK Lasers

Dec 5, 2012

RUGBY, United Kingdom, Dec. 5, 2012 /PRNewswire/ -- JK Lasers (the "Company", "we", "our", "JK"), a division of GSI Group Inc., announced the launch of a new powerful 3 kilowatt (kW) fiber laser for industrial material processing. The new addition to the Company's range of watt to kilowatt (kW) fiber lasers will help enhance manufacturing productivity by processing metals at faster speeds and to higher standards.

(Logo: http://photos.prnewswire.com/prnh/20120305/NE64445LOGO )
(Logo: http://photos.prnewswire.com/prnh/20121205/NE24935LOGO )

Delivering stable output power from switch on, the JK3000FL features a consistent focused spot size and beam profile over the complete power range.  It is fitted with JK Lasers' detachable "plug in, pre-aligned" (PIPA) beam delivery fibers, offering core diameters from 100µm, providing maximum versatility when processing difficult to access areas.

The launch of JK Lasers' JK3000FL has helped to open up new applications for the company, including remote laser welding, typically used in high volume automotive assemblies.  This application has previously been dominated by high power CO2 lasers that use a high brightness laser source and scan head to project the focused spot over a few meters. 

Compared to Nd:YAG lasers of a similar power level, the JK3000FL is up to ten times more energy efficient. It is also highly reliable, with a 300,000 hour mean time to failure (MTTF) of the individual laser pump sources, contributing to extended system lifetimes and uptime.  Other benefits of the JK3000FL include user-friendly software, fast modulation, pulse shaping and JK Lasers' patented back reflection protection. This unique system protects the laser from damaging reflected light when processing highly reflective materials such as aluminum, copper, brass and gold.

The JK3000FL can also be fitted with JK Lasers' own range of process tools for optimal performance and an optional timeshare unit that can rapidly connect up to four separate workstations.

For more information about the JK3000FL, please call +44 (0) 1788 517800, or email sales@jklasers.com, or visit www.jklasers.com.

About the Companies

JK Lasers, a division of GSI Group Inc. and a leading supplier of fiber lasers, Nd:YAG laser solutions, Q-Switched Lasers, Gas Lasers, and associated process tools.  The company is based in Rugby, U.K. and has been in business for more than 40 years.  

More information about JK Lasers' fiber laser range is available on the company's website at www.jklasers.com.  For additional information, please contact JK Lasers, sales on +44-(0)1788-517800 or email sales@jklasers.com.

GSI Group Inc. designs, develops, manufactures and sells laser-based solutions, optical control devices and associated precision motion technologies to electronics, industrial, medical, and scientific markets. GSI Group Inc.'s common shares are quoted on NASDAQ (GSIG).

Safe Harbor and Forward Looking Information

Certain statements in this release are "forward-looking statements" within the meaning of the Private Securities Litigation Reform Act of 1995 and are based on current expectations and assumptions that are subject to risks and uncertainties. All statements contained in this news release that do not relate to matters of historical fact should be considered forward-looking statements, and are generally identified by words such as "expect," "intend," "anticipate," "estimate," "plan," "aim," and other similar expressions.

These forward-looking statements are neither promises nor guarantees, but involve risks and uncertainties that may cause actual results to differ materially from those contained in the forward-looking statements. Our actual results could differ materially from those anticipated in these forward-looking statements for many reasons.  A list of these and other important risk factors that could affect the outcome of the events set forth in these statements and that could affect the GSI Group's operating results and financial condition are discussed in Item 1A of our Annual Report on Form 10-K for the fiscal year ended December 31, 2011, and in the Company's subsequent filings with the SEC made prior to or after the date hereof. Such statements are based on the Company's management's beliefs and assumptions and on information currently available to the Company's management. The Company disclaims any obligation to update any forward-looking statements as a result of developments occurring after the date of this document except as required by law.

SOURCE GSI Group Inc.


print email rss